This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: FLS Module for Autosar

Part Number: TMS570LS3137


Hi

In the Autosar MCAL provided for the TMS570LS3137, we have the FEE module to integrate for non volatile memory.

That's fine when using the internal flash EEPROM of the CPU.

However, our applicaiton requires us to use an external flash because of the size of the data we need to store and storage frequency.

Is there an existing autosar compliant FLS module that would integrate with a third party FEE module and target an external flash on SPI ? Or do we have to code it from scratch ?

Thanks for pointing us into the right direction.

Regards

Seb