Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: TM4C1294NCPDT
In TM4C1294NCPDT, I am using TivaWare's SysCtl Delay to use a 1 second delay, but it is not stable at 1 second or several hundred ms each time the power is turned on.
Please teach me if there are any prerequisites for using SysCtlDelay. The code itself is a simple code that blinks the LED every second as shown below.
The operating frequency is set to 120MHz.
------
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
while(1)
{
i32usr = SysCtlClockGet()/3;
ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, GPIO_PIN_0); /* LED4-ON */
SysCtlDelay(SysCtlClockGet() / 3); // delay 1 second
ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0U); /* LED4-OFF */
SysCtlDelay(SysCtlClockGet() / 3); // delay 1 second
}
-----
Thanks,
Astro