Part Number: AM2432
Other Parts Discussed in Thread: AM2431, DRA821U
Hi Team,
My customer has questions regarding the IBIS model.
- Looking into IBIS model(sprm730.ibs), there are two variations "LVCMOS_H" and "LVCMOS_V" for LVCMOS model. what's the difference between them? For example, PRG0_PRU1 GPO9 pin attaches LVCMOS_H model, but PRG1_PRU0_GPO0 attaches LVCMOS_V model in the sprm730.ibs.
On AM2431 datasheet, Table 6-1. Pin Attributes (ALV, ALX Packages) (continued), I compared the details of PRG0_PRU1_GPO9 and PRG1_PRU0_GPO0. it seems that the difference is only Power domain(VDDSHV1 or VDDSHV2). Are there any other factors contributing to the difference? -
Looking into IBIS model(sprm730.ibs), it seems that there are six variatons for LVCMOS_H (1.8V/3.3V x Nom/slow/Fast). Which one should I use for the simulation?
|********** LVCMOS
[Model Selector] LVCMOS_H
lvcmos1_nom_1p8_h PRWDWUWSWEWCDGLVCMOS_H@_Nom_1p8_comment
lvcmos1_nom_3p3_h PRWDWUWSWEWCDGLVCMOS_H@_Nom_3p3_comment
lvcmos1_slow_1p8_h PRWDWUWSWEWCDGLVCMOS_H@_Slow_1p8_comment
lvcmos1_slow_3p3_h PRWDWUWSWEWCDGLVCMOS_H@_Slow_3p3_comment
lvcmos1_fast_1p8_h PRWDWUWSWEWCDGLVCMOS_H@_Fast_1p8_comment
lvcmos1_fast_3p3_h PRWDWUWSWEWCDGLVCMOS_H@_Fast_3p3_commentI found a related post on TI E2E.
e2e.ti.com/.../dra821u-does-the-ibis-model-work-with-the-drv_str-setting
DRA821U: Does the ibis model work with the DRV_STR setting? - Processors forum - Processors - TI E2E support forumsIt mentions about another device, but it says I can use the model which set on the DRV_STR bit on padconfig register.
In the answer of another Q&A(no.86), We should set DRV_STR as 00b. Does that mean we use Nom model for the simulation?
I expect that We can choose Slow model(set DRV_STR the value of "Slow" driver-strength). because there are models for Slow-driver. Considering signal rate and PWB design, I'd like to use slow driver for output pin.
Best regards,
Mari Tsunoda