Part Number: TM4C129XNCZAD
Hi,
I'm using:
CCS : Version: 9.3.0.00012
XDCTool : xdctools_3_32_01_22_core
ARM Compiler : ti-cgt-arm_18.12.5.LTS
TIRTOS : tirtos_tivac_2_16_01_14
I have a code that I tried to separate part of it in a static library, but I was surprised that after doing this, the over all code increased by 8K.
after some investigations, I found that some of the functions that are implemented in the library and it wasn't invoked by the main code, the linker included it in the code. and this isn't the case where all the code was in one project.
Is there a way to let the linker ignore the unused function in the library to save the code space?
Thanks,
Mohammed