Part Number: TMS570LC4357
王工您好:
安全手册中,7.97 PLL Slip Detector。
在我们使用570过程中,是需要自己去触发PLL Slip并看ESM模块能否检测到此Slip,还是我们直接程序监控ESM模块是否存在PLL Slip错误?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
王工您好:
安全手册中,7.97 PLL Slip Detector。
在我们使用570过程中,是需要自己去触发PLL Slip并看ESM模块能否检测到此Slip,还是我们直接程序监控ESM模块是否存在PLL Slip错误?
Hi MingXi,
You can do both:
1. The PLL slip monitoring circuit monitors the PLLSLIP in run time. Whenever the PLL slip occurs, the flag in GLBSTAT register and ESM should be set. If ROS is set, a reset is generated.
2. You can force a PLL slip to check if an expected error is generated (flags in global status register, and ESM 1.10 and ESM 1.42)
王工:
在FMEDA计算中,针对PLL slip detector,我们如果是想将这项设置为1。
是因为570的ESM模块可以检测PLL slip 还是我们需要You can force a PLL slip to check if an expected error is generated 。

This is to test the PLL slip detection logic. You need to force a PLL slip to check if an expected error is generated