Part Number: TMS570LS1115
1.What is the tolerance range of the external pin filter capacitor for tms570ls1115 chip 1.2V core power supply?
2. Is there no requirement for 1.2V and 3.3V power on sequence as stated in the specification?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS1115
1.What is the tolerance range of the external pin filter capacitor for tms570ls1115 chip 1.2V core power supply?
2. Is there no requirement for 1.2V and 3.3V power on sequence as stated in the specification?
Hi Sam,
1. You can 100nF, 10nF, or even bigger capacitor on the power pins. The basic function of the decoupling or bypass capacitor is to reduce voltage spikes on the power pin.
2. No. The device has a built-in VMON module. The VMON will handle the power sequence of the 1.2V and 3.3V