Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN
Dear TI-Support,
The adc1 group1 trigger is synchronized with a specific PWM signal and the ADC is running at a cycle time of 62.5ns. There are more than 5 inputs signals in this ADC group. In short, I need to know exactly how much time the ADC will need to sample the input signal 3.
I'm having doubts on how to compute the exact time for an input sample to be obtained. According to Halcogen, the following variables shall be taken into account: total scan (Tscan), time to discharge the capacitor (tDischarge), time to sample (tSample) and time to convert the signal (tConversion). I can't find any explanation or guide on how these variables intertwine with each other and what's their actual sequence.
Some questions I have regarding the sampling sequence:
- Are all input signals scanned first before anything else?
- What is the scan period used for?
Assuming that the continuous conversion is disabled and that there is no discharge time for the internal capacitor, how much time will it take for input signal 3 be sampled? As I see it there are three options:
- 3 * ( tScan + tSample )
- 3 * ( tScan + tSample ) + 2 * tConversion
- total tScan + 3 * tSample
- total tScan + 3 * tSample + 2 * tConversion

Thanks for the support