This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert
SDK: MCU-PLUS-SDK-AM263X_08_02_00_28
we use sbl_prebuilt\am263x-cc\ sbl_qspi.release.tiimage to load appimage with 217KB size.
After power on, show sbl log for SBL Total Time Taken almost ~200ms, but our customer requirement is <100ms
Our QSPI IC is same as AM263X-CC EVM
please guide us how to reduce sbl time for QSPI booloader?
BR
JAY
Hi Jay,
We have enabled DMA mode support in SBL which has reduced the boot time drastically. This would be part of SDK8.3 release (planned in next week).
Below is boot time with new updated SBL -
PP Image: hello_world_am263x-cc_r5fss0-0_nortos_ti-arm-clang_458752.appimage
Size: 488KB
Platform AM263X-LP
Starting QSPI Bootloader ...
[BOOTLOADER PROFILE] System_init : 795us
[BOOTLOADER PROFILE] Drivers_open : 35us
[BOOTLOADER PROFILE] Board_driversOpen : 262us
[BOOTLOADER PROFILE] CPU load : 28224us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 29317us
Image loading done, switching to application ...
Hello World! From Bucher
GPIO LED Blink Test Started ...
GPIO LED Blink Test Passed!!
All tests have passed!!
Regards,
Prasad