Part Number: TM4C129XNCZAD
Hi ,
Is there a way to re-initialize the USB without powering it off and on again?
Thank you.
The way I use it is as follows:
#define SYS_CLOCK_FREQ 120000000
#define USB_PLL_CLOCK 480000000
void USBCDCD_reinit(void)
{
uint32_t ui32PLLRate, g_ui32SysClock;
g_ui32SysClock = SYS_CLOCK_FREQ;
ui32PLLRate = USB_PLL_CLOCK;
state = USBCDCD_STATE_UNCONFIGURED;
SysCtlPeripheralDisable(SYSCTL_PERIPH_USB0);
SysCtlUSBPLLDisable();
SysCtlDelay(4800000);
SysCtlUSBPLLEnable();
SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0);
SysCtlDelay(1000000);
g_ui32SysClock = SYS_CLOCK_FREQ;
ui32PLLRate = USB_PLL_CLOCK;
USBDCDFeatureSet(0, USBLIB_FEATURE_CPUCLK, &g_ui32SysClock);
USBDCDFeatureSet(0, USBLIB_FEATURE_USBPLL, &ui32PLLRate);
USBStackModeSet(0, eUSBModeForceDevice, 0);
}
Ray Yang