Part Number: TMS570LS3137
Can I know whether TMS570LS3137ZWT MCU and RM48L952DZWTT MCU are pin to pin compatible or not?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3137
Can I know whether TMS570LS3137ZWT MCU and RM48L952DZWTT MCU are pin to pin compatible or not?
Hi,
Yes, they pin to pin compatible. But those two packages don't have exactly the same peripherals.
For example, the Flexray module is not supported by RM48Lx, but is supported by TMS570LS31x
The RM48Lx supports USB host and device modules, but TMS570LS31x does not support.
The operating temperature for two devices are also different:
RM48Lx: –40ºC to 105ºC
TMS570LS31x: –40ºC to 125ºC