Part Number: TMS570LC4357
Hey,
I am currently trying to debug the ESM interrupt behavior of the TMS570LC4357 using a Lauterbach setup (Powertrace 3 + Power Debug Pro + Preprocessor Autofocus 2). In more detail I am writing a non zero value to the Polarityinvert Register of the R5-CCM module to force a core compare mismatch which would lead to the ESM Group 2 being triggered on channel 2. The behavior works perfectly fine and as expected when debugging with CCS, however once I connect the Lauterbach to use Trace32 the esmGroup2 handler is not being called anymore and the error LED is not being toggled. The coded does reach the point of setting the Polarityinvert Register though. Even when flashing the board trough the Powertrace the LED starts blinking again when I disconnect the Powertrace and powercycle the board so I assume the software is flashed correctly.
Is the Lautebach effecting the ESM or CCM module? Am I missing something? I've tried to find more info on it but could not find anything indicating that using Trace32 would have any effect on this error detection mechanism.
Thanks in advance,
Alex