Part Number: AM2432
Hi Team,
My customer has a question below regarding LVCMOS.
- About 7.7.7 LVCMOS Electrical Characteristics 3.3-V MODE in datasheet.
The table says.
MIN value of IOL is 5mA, and MIN value of IOH is 9mA
Are those correct?
It seems that they means sink or source current value of logic output pin. Generally MAX values are defined for those parameters. Am I correct?
Best regards,
Mari Tsunoda