Part Number: TM4C1292NCPDT
Other Parts Discussed in Thread: TM4C1294NCPDT
Hi,
I am using 25mHZ crystal and trying to configure microcontroller with following API.
output_clock_rate_hz = MAP_SysCtlClockFreqSet(
(SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL | SYSCTL_CFG_VCO_240),
SYSTEM_CLOCK);
But this function is crashing at line 2320 (TivaWare_C_Series-2.2.0.295 )
//
// Set the oscillator source.
//
HWREG(SYSCTL_RSCLKCFG) |= ui32OscSelect;
The value in ui32OscSelect is 0x03300000. I am using the same function for tm4c1294ncpdt it works fine. HW wise clock section has same design for tm4c1292 and tm4c1294.
Is it a known issue or am I missing something ? I am using tivaware (TivaWare_C_Series-2.2.0.295 ). What is the solution or suggestion
Regards,
Parvez Akhtar