Part Number: TMS570LC4357
王工您好:
tms570进行pbist自检,完成后需要进行ram重新初始化吗?如果需要的话,需要重新初始化哪些ram?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mingxi,
tms570进行pbist自检,完成后需要进行ram重新初始化吗?
Yes, TI recommends that the PBIST routines be executed on the SRAM prior to the auto-initialization.
如果需要的话,需要重新初始化哪些ram?
The RAM group to which you have performed the PBIST.
王工:
我看HL_sys_startup.c里面,poweron_reset后需要初始化L2RAM,来避免ECC错误。
我想问一下,如果不执行_memInit_()的话,一定会产生ECC错误吗?如果产生了,在ESM的GROUP几能监控到呢?
case POWERON_RESET:
/* Initialize L2RAM to avoid ECC errors right after power on */
_memInit_();
如果不执行_memInit_()的话,一定会产生ECC错误吗?
如果有ECC问题,一定会被检测到。
如果产生了,在ESM的GROUP几能监控到呢?
可以检测到。具体是哪个ESM group,要看情况。有可能是EPC ESM1.4, or 2.21. 你得到的是什么?