Part Number: MCU-PLUS-SDK-AM263X
Hi,
I'm using AM263x-cc EVM with SDK version "mcu_plus_sdk_am263x_08_02_01_08".
I want to check the EST effect with UDP or TCP protocol.
Hence, I integrated the example est+lwip, and also enabled vlan tag and pcp in lwip.
Now I can send udp packet with different pcp, but it seems the packet transmission time doesn't meet the gate control setting.
My gate control setting list below:

And I also attach the packet capture file for your reference:
AM26EVM_LWIP_EST_500us_Cycle.zip
I sent udp packet with pcp 0,2,4,6 recursively in the same time.
Do you have any suggestion about my test?
Thanks,
Josh