Part Number: MCU-PLUS-SDK-AM243X
How can I use SBL's memory from application once it is done executing as it will be wasted otherwise?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MCU-PLUS-SDK-AM243X
How can I use SBL's memory from application once it is done executing as it will be wasted otherwise?
Hi,
You can use the SBL memory in primary R5's application by allocating it to a uninitialized sections (NOLOAD) section.
Steps to do that -
1. Define MSRAM_SBL section in Primary R5Fs app
/* SBL used memory, use only for uninitalized sections */ MSRAM_SBL : ORIGIN = 0x70000000 , LENGTH = 0x60000
2. Allocate uninitialized/NOLOAD sections like .bss, .stack to this newly created section
/* This is rest of uninitialized data. This can be placed in DDR if DDR is available and needed */
GROUP {
.bss: {} palign(8) /* This is where uninitialized globals go */
RUN_START(__BSS_START)
RUN_END(__BSS_END)
.sysmem: {} palign(8) /* This is where the malloc heap goes */
.stack: {} palign(8) /* This is where the main() stack goes */
} > MSRAM_SBL
3. Confirm from the memory map file, the allocation of uninitialized sections. Check the UNINITILIAZED section attribute at the beginning.
.bss 0 70000000 00001498 UNINITIALIZED
70000000 00001008 (.common:gHwiCtrl)
70001008 00000280 ti_drivers_config.o (.bss.gUartObjects)
70001288 00000120 libsysbm.a : trgmsg.c.obj (.bss:_CIOBUF_)
700013a8 000000a0 (.common:__TI_tmpnams)
70001448 00000038 (.common:gClockCtrl)
70001480 00000008 (.common:parmbuf)
70001488 00000004 nortos.am243x.r5f.ti-arm-clang.debug.lib : HwiP_armv7r_vim.obj (.bss.gdummy)
7000148c 00000004 libc.a : memory.c.obj (.bss.sys_free)
70001490 00000004 (.common:gUartHandle)
70001494 00000004 --HOLE--
.sysmem 0 70001498 00008000 UNINITIALIZED
70001498 00000010 libc.a : memory.c.obj (.sysmem)
700014a8 00007ff0 --HOLE--
.stack 0 70009498 00004000 UNINITIALIZED
70009498 00000004 nortos.am243x.r5f.ti-arm-clang.debug.lib : boot_armv7r_asm.obj (.stack)
7000949c 00003ffc --HOLE--
Some points to note:
Hope this helps!
Regards,
Prasad