This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: test connector pinout

Part Number: LP-AM243


I would like to make a breakout board for the test automation connector of the LP-AM243x, but I am puzzled by the documentation.

The documentation says (section 4.16):

The LaunchPad supports a 40-pin test automation header (687140183622 from Wurth).

The Wurth connector and the associated flat-panel connector are indeed 40 pins, according to their datasheets.

But table 4-16 shows 42 pins, not 40.

Is this an error?

I can't find a schematic for the LP-AM243, otherwise I'd just look at the Gerbers or schematics and figure this out myself.

Thanks,
--Terry