Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
My customer asked two questions below regarding sysconfig.
- About sysconfig, MMCSD setting (see image), I think the pin direction for each pin is uniquely defined by terminals. Why is the Rx checkbox of each pin selectable?
- "MMC1_CMD" is output signal, but I can check RX checkbox manually.
- "MMC1_DAT[3:0]" are bi-direction signal, but I can uncheck RX checkbox manually.
- Rx checkbox of "MMC1_SDCD" is fixed to be checked.
- "MMC1_CLK" is output signal, but I cannot uncheck the Rx checkbox. because it's gray-outed and fixed to be checked.

- About sysconfig, Enet(CPSW) setting (see image below) We are going to use RMII1_* signals and not going to use RMII2_* signal. In this case, is the following correct?
- Disable Mac port1 checkbox: not checked
- Disable Mac port2 checkbox: checked
- (I have this question because I checked "Disable Mac Port2" checkbox, and RMII2_* signals checkbox, but no error occurred.)

Best regards,
Mari Tsunoda