Part Number: HALCOGEN
Other Parts Discussed in Thread: TMS570LC4357
Hello,
I have a question on the available diagnostics provided by HALCoGen (04.07.01) for the Hercules TMS570LC4x.
I am using the TMS570LC4357 and the "Safety Manual for TMS570LC4x Hercules ARM Safety MCUs" (SPNU540A) specifies, in table4, the following diagnostics for most of the device partitions within the microcontroller.
- 7.94 Periodic Software Read Back of Static Configuration Registers
- 7.118 Software Read Back of Written Configuration
For many of the device partitions HALCoGen generates functions of the form xxxGetConfigValue() to perform these two diagnostics. e.g. esmGetConfigValue()
However, for the following device partitions, no HALCoGen generated functions of the form xxxGetConfigValue() exist, even though the Safety Manual states that the Configuration Registers for each device partition can be checked by these two diagnostics.
Reset - RST6 & RST7
Primary Flash - FLA8 & FLA9
Flash EEPROM Emulation (FEE) - FEE5 & FEE6
Primary SRAM - RAM10 & RAM11
CPU Interconnect Subsystem - MEM4 & MEM6
Peripheral Interconnect Subsystem - PER4 & PER6
Peripheral Central Resource 1 - P1T4 & P1T6
Peripheral Central Resource 2 - P2T4 & P2T6
Peripheral Central Resource 3 - P3T4 & P3T6
Vectored Interrupt Module - VIM6 & VIM7
Error Profiling Controller - EPC1 & EPC3
So how are the "Periodic Software Read Back of Static Configuration Registers" and "Software Read Back of Written Configuration" diagnostics performed on each of the the above 11 device partitions?
Thank you.