Part Number: MSP432E401Y
Other Parts Discussed in Thread: SYSCONFIG
I am working to build an RTD interface from scratch as many of the all-in-one solutions are out of stock and I believe the MSP432 should have the ADC resources to handle it. I am working from TI's "A Basic Guide to RTD Measurements" Section 2.4 - Three wire RTD with a single IDAC source, as well as referencing a circuit note from Analog Designs (sorry to mention a competitor)
The two questions I have about the ADCBuffer driver are:
1. Does the "Reference Voltage" option in the Sequencer Channel submenu of the sysconfig for ADCBuffer only affect the "convertAdjustedtoMicroVolts" function output?
2. If I were to set up measurements for three 3-wire RTDs I would need 6 differential pairs - would this be done with 3 ADC buffers, or one ADC buffer with 6 channels of sequencer 0 set up to fill out individual buffers for each differential pair? Could either work?
As a side note, I noticed that adjustRawValues implementation for the MSP432 does not edit any values because there is no calibration feature for the ADC, is my understanding correct?
I am working off of the example code ADBufDifferential.c to retrieve the voltages from the differential measurement and then carrying out the conversion per the Guide to RTD measurements to end up with a measured resistance for the RTD. With that I plan to use the Callender-Van Dusen equation to retrieve temperature.
My first prototype implementation of this did yield a promising result, but I'm hoping it isn't a fluke.
Many thanks for the support,
Darren