Part Number: AM2431
As USB feature on AM2431, my customer is asking about following questions.
1. Is the USB Host controller compatible with EHCI?
2. Does it have a SOF trigger function?
They plan to use this function that activates the internal timer as a trigger.
For example, When internal timer reaches a certain , start start UART DMA for data transmission.