This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357-EP: RoHS Compliance

Part Number: TMS570LC4357-EP


Hi there,

I'm currently supporting the design of a new avionics system and we're in the part selection phase of the project. A requirement for the product is that it can operate at -55 C, but also that we use RoHS compliant parts. I see that a SnPb solder is the only option that is offered on the TMS570LC4357-EP and it says it is not RoHS compliant. Is this the only reason that the -EP is not RoHS compliant? Is using SnPb solder the reason that the TMS570CL4357-EP has an extended operation range to -55 C from the standard part that stops at -40 C or are the parts binned in some way? 

Thanks!