This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: Connecting XDS200 Debug Probe

Part Number: RM57L843

Hello,

A team member is designing a PCB for a new product based around the TI RM57L843 but we are having issues connecting to the debug probe.  I have connected using the 20-pin (2.54mm pitch, labelled 20eCTI - 20ARM on the silkscreen) ARM probe adaptor and have all signals connected except DBGRQ and DBGACK.  When trying to verify the connection in Code Composer I get an error, full output window at bottom of message.

Am I using the incorrect adaptor or is there something else going on?  I have tried with and without 4.7K pull ups on TDI/TMS and nReset and a 4.7k pull downs on TCK.

XDS200 end connections were assumed from the ARM-20 Pin column on dev.ti.com/.../node

Any help would be gratefully received.

Thank you,

Craig.

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\CRAIG~1.OVE\AppData\Local\TEXASI~1\
CCS\ccs1120\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Mar 17 2022'.
The library build time was '19:20:23'.
The library package version is '9.7.0.00213'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

This emulator does not create a reset log-file.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

[End]