This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Error compiling SBL_NULL example

Part Number: AM2634

I am getting the following error compiler the SBL_NULL example included in    ...mcu_plus_sdk_am263x_08_03_00_23\examples\drivers\boot\sbl_null. Following is the output from CCS12. Could someone guide what I should be looking at

C:/ti/ccs1200/ccs/utils/bin/gmake -C C:\Users\rdsouza\workspace_v12\sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang -f makefile_ccs_bootimage_gen OUTNAME=sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang PROFILE=Debug MCU_PLUS_SDK_PATH=C:/ti/mcu_plus_sdk_am263x_08_03_00_23 CG_TOOL_ROOT=C:/ti/ti_cgt_tiarmclang_1.3.1.LTS CCS_INSTALL_DIR=C:\ti\ccs1200\ccs CCS_IDE_MODE=desktop
Boot image: am263x:r5fss0-0:nortos:ti-arm-clang C:/Users/rdsouza/workspace_v12/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang/Debug/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang.tiimage ...
C:\ti\ccs1200\ccs/utils/tiobj2bin/tiobj2bin Debug/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang.out C:/Users/rdsouza/workspace_v12/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang/Debug/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang.bin C:\ti\ccs1200\ccs/tools/compiler/ti-cgt-armllvm_1.3.1.LTS/bin/tiarmofd C:\ti\ccs1200\ccs/tools/compiler/ti-cgt-armllvm_1.3.1.LTS/bin/tiarmhex C:\ti\ccs1200\ccs/utils/tiobj2bin/mkhex4bin
C:\ti\ccs1200\ccs/utils/tiobj2bin/mkhex4bin failure occurred. Giving up.
python C:/ti/mcu_plus_sdk_am263x_08_03_00_23/tools/boot/signing/mcu_rom_image_gen.py --image-bin C:/Users/rdsouza/workspace_v12/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang/Debug/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang.bin --core R5 --swrv 1 --loadaddr 0x70002000 --sign-key C:/ti/mcu_plus_sdk_am263x_08_03_00_23/tools/boot/signing/mcu_gpkey.pem --out-image C:/Users/rdsouza/workspace_v12/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang/Debug/sbl_null_am263x-lp_r5fss0-0_nortos_ti-arm-clang.tiimage --debug DBG_SOC_DEFAULT
makefile_ccs_bootimage_gen:59: recipe for target 'all' failed
The system cannot find the path specified.
File does not exist: at XML_TI_OFD.pm line 877.
Traceback (most recent call last):
File "C:\ti\mcu_plus_sdk_am263x_08_03_00_23\tools\boot\signing\mcu_rom_image_gen.py", line 148, in <module>
cert_str = get_cert(args)
File "C:\ti\mcu_plus_sdk_am263x_08_03_00_23\tools\boot\signing\mcu_rom_image_gen.py", line 124, in get_cert
IMAGE_LENGTH = os.path.getsize(args.image_bin),
File "C:\Users\rdsouza\AppData\Local\Programs\Python\Python310\lib\genericpath.py", line 50, in getsize
return os.stat(filename).st_size
gmake[3]: *** [all] Error 1
gmake[2]: [post-build] Error 2 (ignored)
makefile:178: recipe for target 'post-build' failed

Thank you

Royston