This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Heap memory in Map file



Hello,

We have recently changed compiler to ti-cgt-armllvm_1.3.1.LTS and it comes with default gmake build system. We have migrated the software to cmake due to project requirements. i have passed same options in cmake as of gmake. but observed that there is heap memory(.sysmem) getting added. 

in gmake, linker option takes heap_size as 8k and same in cmake also but gmake doesnt contain heap memory in map file while cmake map file does. i understand that due to llibc.a memory.c file getting referenced in cmake which is creating heap. 

-llibc.a option in linker means which libc.a file in compiler folder. i see there are multiple options available. 

compiler\ti-cgt-armllvm_1.3.1.LTS\lib\libc.a or compiler\ti-cgt-armllvm_1.3.1.LTS\lib\armv7r-ti-none-eabi\c\libc.a.

currently i have added second option as library which seems to complete the build but creates heap. but if i add first option as library then build will fail due to unknown references. 

Please help me identify which libc.a to include as library so that i can complete build without any heap just as gmake output. Please let me know if you need any further input from my end. 

Thank you