Part Number: TMS570LS3137
Hello, I am changing the start address of the main application for my bootloader application and loading the code with the compiler, but the red led is on. I think I need to change the vector offset value, but I couldn't find anything about it. Can you help me how can I fix this problem?
/* */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Linker Settings */
--retain="*(.intvecs)"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
/* USER CODE BEGIN (2) */
FLASH_BOOTLOADER (RX) : origin=0x00000020 length=0x0017FFE0
VECTORS (X) : origin=0x00180000 length=0x00000020
FLASH_APPLICATION (RX) : origin=0x00180020 length=0x0017FFE0
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0003EB00
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
/* USER CODE BEGIN (4) */
.intvecs : {} > VECTORS
.text : {} > FLASH_APPLICATION
.const : {} > FLASH_APPLICATION
.cinit : {} > FLASH_APPLICATION
.pinit : {} > FLASH_APPLICATION
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
/* USER CODE END */
}
/* USER CODE BEGIN (5) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Misc */
/* USER CODE BEGIN (6) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/