Part Number: TM4C123GH6PM
Hello,
I am attempting to use the QEI module to interface with a rotary encoder ( with pushbutton) that I want to use as an input device to a small embedded project. much like a volume knob on a car radio but the rotation would be used to increment and decremnt an on screen menu and the pushbutton would indicate the selection. My initial run at this is noisy and I can deal with that. but i do have a couple questions.
the part in question at digi key.
ACZ11BR1E-20KQD1-20C |
|---|
Is this a good fit? this device and the QEI module. seems made to order.
why the lack of example code for the QEI module. Surprisingly few examples from TI . Noticed github is also pretty bare of such examples.
Part of why I am questioning the design path.
Thanks
Pat