Part Number: TM4C1294NCPDT
I was using the suggested code shared in other posts to print float numbers, splitting it in an integer and a fraction part:
void FloatTo2PartInteger(float IntegerToConvert, int32_t* IntegerPart, int32_t* FractionPart){
*IntegerPart = (int32_t) IntegerToConvert; // Convert IntegerPart from float number
*FractionPart = (int32_t) (IntegerToConvert * 10.0f); // Convert FractionPart from float number
*FractionPart = *FractionPart - (*IntegerPart)*10; // Remove IntegerPart from FractionPart
if (*FractionPart < 0) { // If FractionPart is negative
*FractionPart *= -1; // Multiply itself per -1 to obtain positive part
}
}
But I have observed it is not printing the negative signal for numbers inside the range [-1... 0]. Example: When I was trying to print the number -0.063 I have 0.063 with no negative signal.
Here a suggested code to fix it:
void PrintFloat(float finput, uint8_t *ui8Sign, int32_t *i32IntegerPart, int32_t *i32FractionPart) {
//
// Convert the floating point input to an integer part
// and fraction part for easy printing.
//
*i32IntegerPart = (int32_t)finput;
*i32FractionPart = (int32_t)(finput * 1000.0f);
*i32FractionPart = *i32FractionPart - (*i32IntegerPart * 1000);
if(*i32FractionPart < 0) {
*i32FractionPart *= -1;
if(*i32IntegerPart == 0) {
*ui8Sign = 0x2D;
}
}
else {
*ui8Sign = 0x00;
}
}
And here an use example:
PrintFloat(fADISData[3], &ui8Sign, &i32IntegerPart, &i32FractionPart);
UARTprintf("X_ACCEL: %c%d.%03d ", ui8Sign, i32IntegerPart, i32FractionPart);
I think the problem was, when the integer part is zero it is not possible to hold the sign information.