Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Dear Champs,
My customer is trying to test XIP and they can run LWIP example successfully without FLASH driver in sysconfig.
But, when they add FLASH driver in sysconfig as below, they found the LWIP example was stuck after boot success print out.
Could you please let me know if it is normal to add flash driver in sysconfig when XIP was used?
They made XIP image according to below UG and flash it into flash memory using UART uniflash. And then, they reboot EVM with QSPI boot mode.
They added FLASH driver in sysconfig as below.

Thanks and Best Regards,
SI.