Part Number: LAUNCHXL2-TMS57012
Other Parts Discussed in Thread: BQ76PL455EVM, HALCOGEN
I have currently on a BMS project using LAUNCHXL2-TMS57012 as controller and BQ76PL455EVM as battery sensing.
I have successfully communicate with BQ76PL455EVM/BQ79616EVM through SCI1 port of LAUNCHXL2-TMS57012.
HALCOGEN Setup steps:
1. RTI,GIP, SCI Driver enabled.
2. In SCI section RX_INT Enabled (receive interrupt enabled). Baurdrate: 250000 (for BQ76PL455EVM )
3. In VIM channel section, RTI Compare 1 and SCI level 0 interrupt enabled.
As per sample code of BQ76PL455EVM, the required source and header files are included in this project, and made required changes in PL455.c source file for SCI.
I am able to receive the cell voltage data.

However, when I set it for SCI2(LIN) port. I am unable receive data from BQ76PL455EVM. For SCI2, I have made required changes in Halcogen and PL455.c source file.
Q1. Is it possible to use SCI2 port to communicated BQ76PL455EVM or not?
Q2. Is there any specific changes needed in hardware for SCI2?