Part Number: TMS570LC4357
I have a question on the default power domain states of the Hercules TMS570LC4x.
I am using the TMS570LC4357 and section 5.3.2 Default Power Domain State for the Power Management Module (PMM) in the Technical Reference Manual TMS570LC43x 16/32-Bit RISC Flash Microcontroller (SPNU563A March 2018) states that "The default state of each power domain, except for PD1, is controlled by TI during production testing via programmation of individual bits within the reset configuration word in the TI-OTP sector of flash bank 0."
The OTP Memory is described in section 7.5.2, but the default state of each power domain is not defined.
What are the default states of each power domain?