Part Number: TMDSEMU110-ETH
Other Parts Discussed in Thread: TMDSEMU110-U, TMS320F28069
Hi,
Can I use the TMDSEMU110-ETH debugger for flashing the c2000 controller family instead of
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSEMU110-ETH
Other Parts Discussed in Thread: TMDSEMU110-U, TMS320F28069
Hi,
Can I use the TMDSEMU110-ETH debugger for flashing the c2000 controller family instead of
Rohit,
Yes, it will support C2000 devices.
https://www.ti.com/tool/TMDSEMU110-ETH

Thanks & Regards,
Santosh
Hi Santosh,
Thank you for the response !!!
As i have mentioned currently in the market TMDSEMU110-U debugger is not available so can i use TMDSEMU110-ETH for flashing the code in our custom design board which is TMS320f28069 controller piccolo family.
If yes then How can i do it ?
Also i have TMDSEMU110-U debugger for that USB port is damaged so with the following arrangement mentioned in the below document can i flash the code in our custom design board
link for the arrangaments : https://www.ti.com/lit/ug/spruie1a/spruie1a.pdf?ts=1663569067964&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FTMDSEMU110-ETH
Thanks & Regards,
Rohit
Rohit,
TMDSEMU110-ETH is add-on package and you need the base unit TMDSEMU110-U to work.
Other option is you can use launchpad of newer devices and then connect the jumper wire from Launchpad to your custom board. It will not be clean solution, but it can be made to work.
https://www.ti.com/tool/LAUNCHXL-F280025C
Schematics:
https://www.ti.com/lit/df/sprr425a/sprr425a.pdf?ts=1663617201014

Thanks & Regards,
Santosh