Part Number: AM2432
Dear Champs,
My customer is implement web server using "enet_lwip_icssg_am243x-lp_r5fss0-0_freertos_ti-arm-clang" example, and trying to have aging test on it.
When there was heavy traffic, they found there was no response from server although process task is still alive and ping occurred.
the log capture is as below.
And also, there was link-down occurred at some time as below.
Could you please check these issues? what should be checked to resolve issue?
~~~~~~~
EnetPhy_bindDriver:1718
Icssg_handleLinkUp:3060
link_callback==UP
5.138s : CPU load = 2.43 %
10.138s : CPU load = 8. 3 %
15.138s : CPU load = 2. 2 %
20.138s : CPU load = 2. 2 %
25.138s : CPU load = 2. 0 %
30.138s : CPU load = 2. 0 %
35.138s : CPU load = 2. 0 %
40.138s : CPU load = 2.44 %
45.138s : CPU load = 2. 0 %
50.138s : CPU load = 2. 0 %
55.138s : CPU load = 2. 1 %
60.138s : CPU load = 2. 0 %
65.138s : CPU load = 2. 0 %
70.138s : CPU load = 2.20 %
75.138s : CPU load = 4.83 %
Icssg_handleLinkDown:3079
link_callback==UP
80.138s : CPU load = 3.92 %
Icssg_handleLinkUp:3060
link_callback==UP
85.138s : CPU load = 2. 5 %
Thanks and Best Regards,
SI.