Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
When I use LM flash to update firmware on the TIV CPU using Ethernet / bootP, the CPU does not execute code after the firmware update until we do a power cycle of the CPU.
I know that when using a probe and not Ethernet, there is a option to reset the CPU after the DFU and with Ethernet this option is grayed out but selected. In other words, I see on the "Program" tab the option "Reset MCU After Program" is selected but the option is grayed out so I can change it. I think this used to work but I have not used these tools in a while.
I am using LM flash build 1613. I know the code is good because it runs after the reset but I would like it to run after its updated without a reset.
Any ideas?
Doug