Hello,
I am using the TMS570LC4357 and I have a question about the selection of the diagnostic mechanisms available on this device.
The "Safety Manual for TMS570LC4x Hercules ARM Safety MCUs" (SPNU540A) section 6.41 Error Profiling Controller (EPC) specifies the following diagnostics:
• Periodic Software Readback of Static Configuration Registers
• Software Readback of Written Configuration
Later in table 4 these are identified as EPC1 and EPC3 respectively.
I thought that a candidate static EPC register for these diagnostics would be EPC REVID Register (EPCREVID) in section 12.4.1 of the Technical Reference Manual TMS570LC43x 16/32-Bit RISC Flash Microcontroller (SPNU563A March 2018).
According to the TRM EPCREVID is entirely read only and its value after a reset is 0x4A0A0000.
However, what I have discovered is that the value of EPCREVID after reset is actually 0x4A0A2000.
Is the TRM out of date in this respect?
Thank you.