Part Number: RM48L950
Hello there
I have a project where I need to use a small het program to measure a gated pulse width modulated signal.
For this I need to program the HET. The problem is, when I try to edit the assembly program in het-idee
the ide freezes and is not possible to work further. I tried on all fresh installed Microsoft Operating systemss including the old Windows 7 and
I had the same issues.
I found on this forum an old post (7 years ago) regarding to this issue and an unofficial patch. Unfortunately the link with the
patch is not available anymore.
Could somebody help me with this issue?
Thank You
HET-IDE V03.05.01
Fri 10/16/2015 14:07:81
The output of the program is the following
Starting the simulator ....
Simulator Constructed Frontend Interface ...
Simulator Listening on Port 50070
Simulator Build Info: Fri 10/16/2015 14:00:08.57
Frontend Connected