Code Composer Studio 11.2.0.00007
Today an update was received automatically for Arm Compiler Tools v20.2.7.LTS. The install path for all TI software is /opt/ti. This includes (showing 2 levels deep):
/opt/ti
├── ccs1120
│ ├── Code Composer Studio 11.2.0.desktop
│ ├── ccs
│ └── xdctools_3_62_01_16_core
└── simplelink_msp432p4_sdk_3_40_01_02
├── changelog.html
├── docs
├── examples
├── imports.mak
├── kernel
├── license_simplelink_msp432p4_sdk_3_40_01_02.txt
├── manifest_simplelink_msp432p4_sdk_3_40_01_02.html
├── release_notes_simplelink_msp432p4_sdk_3_40_01_02.html
├── simplelinkmsp432p4sdk_3_40_01_02.log
├── source
├── tools
├── uninstall
└── uninstall.dat
After installing the update none of my projects would build because the path to /opt/ti was gone from my preferences. This meant the SDK could not be found.
The last time I updated my Linux install (on a fresh hard-drive going from openSUSE Leap 15.0 to 15.4) I installed CCS 11.2. The new install of CCS found the SDK path just fine. All I had to change were the build settings in all projects to use the new 3.40.1.02. My SDK install has always been in /opt/ti, (both under CCS 9.3 on Leap 15.0 and now with CCS 11.2 on Leap 15.4) All projects build setting required update from 3.30.0.13 to 3.40.1.02, but that just required selecting the new version from the drop-down box -- CCS 11.2 knew where it was located.
However after the auto update today to Arm Compiler Tools v20.2.7.LTS, CCS no longer looked in /opt/ti, that config was gone. I had to manually add /opt/ti as a path to search as a Settings -> Code Composer Studio -> Products -> Product discovery path -- something I had never had to do before. Not with either install (CCS 9.3 or 11.2) and not with any version of the SDK I had installed. The setting that was lost and had to be added after update is shown in this screenshot:

This appears to be a bug in the Arm Compiler Tools v20.2.7.LTS update that was auto-installed today. Let me know if there are any logs or anything else I can send (you will probably have to tell me where to look for them). I'm happy to send whatever information you need.