This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: Problem with the SCI and LIN UART of the TMS570LS3137

Part Number: TMS570LS3137


Hello,

I am using Eval board (TMS570LS31X HDK)

I am using both SCI and LIN of TMS570LS3137 but,

1.Not able to send the data through SCI.

2.Not able to receive the data from LIN

Regards,

Rohini 

  • Hi Rohini,

    I would like to know the following things,

    Which instance of SCI is used for SCI and which instance of SCI is used for Lin? I hope you are using two different instances for SCI and Lin instead of implementing on same instance?

    Before combining the both SCI and Lin, did you check them separately, are they working fine when we use only enable either SCI or Lin?

    Can you share your configuration and code if it is disclosable, so that we can easily debug your issue?

    --

    Thanks,

    Jagadish. 

  • Hi,

    Closing the thread because of not hearing back from so long.

    --

    Thanks & regards,
    Jagadish.