Part Number: MCU-PLUS-SDK-AM263X
Hi TI Experts,
I have total 15 Rx messages, which i am currently sending to the ECU on demand (not cyclic) out of which i can see for 11 of them are received properly and the bit 19(DRX) of MCAN0_CFG_IR is getting set, but when i send the rest 4 messages,ISR is triggered but the DRX bit is not set instead the bit 7(RF1L) is getting set.
i am not using Rx Buffers instead of RX FIFO, so its bit strange for me. can some one please guide me if i need to check something else.
Thanks
Bikash