This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kindly suggest me a micro controller



Kindly suggest to me a microcontroller with a baud rate of  230400. And also It needs at least 44  pins to meet our application. It need to be a low-cost microcontroller, we have to procure it locally. Anyway Kindly suggest to me a microcontroller as soon as possible.

  • Hi Aswin,

    What is the peripheral which needs the baud rate of 230400? UART, SPI?

    What kind of pins do you need for your application? GPIO pins?

    Do you have any MIPS (CPU speed) requirement? Any on chip memory requirement?

    Best regards,

    Ming