Part Number: TM4C129ENCPDT
In the TM4C129 series(128-TQFP), there are specifications that are included in Data Protection and others that are not.
Also, are there any problems due to differences in Ethernet specifications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C129ENCPDT
In the TM4C129 series(128-TQFP), there are specifications that are included in Data Protection and others that are not.
Also, are there any problems due to differences in Ethernet specifications?
Hi,
In the TM4C129 series(128-TQFP), there are specifications that are included in Data Protection and others that are not.
I think you are referring to AES/DES/SHA/MD5, right? These are hardware encryption/decryption modules. As far as I know, XDS110 does not use these features.
Also, are there any problems due to differences in Ethernet specifications?
The pinout between the ones with Ethernet will be different from the ones without. I strongly suggest you stay with the same one as on your reference design or EVM board.
Hi, I use this series of ICs to convert from USB protocol to UART protocol.
So I don't think it has much to do with ethernet or data protection.
However, it is better to be careful because the inn placement and role number will change, right?