Hi folks,
I have some questions about the CAN SW Reset on the TMS570. First, am I right to say 'SW' stands for software? My next question is, what happens with the CAN node after the reset?
According to the manual I have to set the Init bit in the control register and after this the SWR bit to perform a SW reset. I have done so, but nothing happens except the bit timing has changed, the interrupts are disabled and the InitDbg bit is set. Is there a difference between a reset in normal mode and debug mode (via CCS)?
Thanks a lot,
Gregor