Part Number: TMS570LS0432
HI,
I use TMS570 MCU CAN Bus functions.
I want do load the CAN ID and data.
how to write the code do to that?

I set the message box9 ID is 0x14EA01EF.

I set the int variable "u32temp" to read the ID,but it can work.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS0432
HI,
I use TMS570 MCU CAN Bus functions.
I want do load the CAN ID and data.
how to write the code do to that?

I set the message box9 ID is 0x14EA01EF.

I set the int variable "u32temp" to read the ID,but it can work.
Hi Kuanlee,
1. You need to transfer the message arbitration or ID from message RAM to IFx register
canREG1->IF1CMD = 0x20U;
canREG1>IF1NO = messageBox;
2. then read the ID from IFx register
u32temp = node->IF1ARB
You can use canGetID(...) in can.c to read the message ID.