Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
I have configured the Timer0 as 64 bit and working in periodic mode. However, the results look like I can only configure the time for the first time to enter the TimerA_IntHandler function. After that, I cannot control the time to enter the TimerA_IntHandler at all. It is always entered the interruption as fast as possible. I wonder if there is any actions which need to be done in the TimerA_IntHandler function so the periodic mode can be continued? Or did I do something wrong in the timer configuration? Thanks.
------------------------------------------
// Configure the Timer.
void ConfigureTimer(void){
//================= timer 0 config 64-bit timers =================
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
// Configure the 64-bit periodic timers
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
// Setup the interrupts for the timer timeout.
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
TimerIntRegister(TIMER0_BASE, TIMER_A,TimerA_IntHandler);
TimerEnable(TIMER0_BASE, TIMER_A);
TimerLoadSet64(TIMER0_BASE, 100000000); // x SEC
}
------------------------------------------