Other Parts Discussed in Thread: HALCOGEN
Good morning, I am trying to communicate data between a Hercules and an ESP-PSRAM64 SPI RAM, for this I have carried out two tests.
The first test was using the normal SPI communication and it was successful, I can write and read data.
the second is to use the MIBSPI communication, I have managed to send the data and also receive data, the latter I can check with my logic analyzer, the problem is that in the internal registers of the microcontroller I have not read anything.
Here you can see that the slave is responding successfully to the master

In the program I do not have any value that the slave sends

These are the configurations of the Halcogen, I am using transfer group 3, to read the data sent by the slave

Could you help me to know the correct configuration.
attached project
My best Regards