Other Parts Discussed in Thread: AM2434
I am attempting to wire up the breakout board to the TMDS243DC01EVM.
Test headers J2 to J9 are missing the pin assignment in Table 3.3.
I cannot correlate the "Net Name" (which corresponds to the "Pin Multiplexed Signal Functions")
to the actual pin assignment on J2 to J9.
Difficult to wire up without this information.
Example:
----------------- EVM Board -----------------||------- Breakout Board ---------------------------
Signal function EPWM0_A is on AM2434 ball U20 --> HSE-E15 --> GPMC0_AD3 --> Mux U11 --> J6-?
Note also the signal name in Table 3-3 probably should have been
GPMC0_AD3 and not GPMC0_ADC3 to be consistent with the name in Table 3-4,
and in document GP EVM User's Guide Table 3-24.