This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Device information checking

Part Number: AM2434

Dear team,

Pls help to check these information for AM2434.

It's very urgent for us to support customer's application.

Thanks

1.Does the MCU Chip include any of the following technologies?
a) Array packages equal to or less than 0.8mm pitch?
b) Ceramic BGA or Cu CGA component
c) Leadless area array component; such as QFN, MLF, LGA, etc.
d) Passives of case size 2512 or larger
2.If the answer to any item in 1 is yes, has solder joint reliability evaluation per IPC9701 on the technology component type(s) been completed?