Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: SCI baud rate setting

Part Number: RM57L843

Hi Team,

VCLK is set to 70MHz. 4 SCIs are used, 3 of which are set to 115200 baud rate (actually 115131). 1 of them is set to 384000 (actually 397727). 

The bit error rate of 384000 is too high. But if customer changes VCLK, the other 3 115200 will be affected. Customer would like to ask if there is another way to set a separate clock for a certain SCI? for baud rate configuration

Thanks,

Annie

  • Hi Annie,

    We can not apply different VCLK's for different instances of SCI. All instances of SCI will operate only on VLCK1 only.
    But there is an another way to do this, i.e. implementing UART on N2HET. There is a way to implement UART on N2HET, u can try that for 384000 baud rate UART. If we did this then all SCI UART instances will operate on VCLK1 and the SCI UART implemented on N2HET will be operate on VCLK2

    Here is an application note to implement UART on N2HET

    Template: Application Report Template (Word)

    Here is an example code on RM46

    N2HET_EMU_UART.zip

    --

    Thanks & Regards,

    Jagadish.