Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN, TCAN337
using the TMS5704357 in a design where it needs to receive extended-ID CAN bus frames with any arbitrary ID Our HALCoGen configuration is shown in the following photo.

You can see in the logic analyzer capture below that there is no ack, which should be provided by the TMS570. I believe that with our HALCoGen config it should ack any frame ID. Why is the TMS570 not sending an ack on these frames? I should also note that the CAN interrupt handler code is not entered at any point.

The TCAN337 IC is being used to interface the MCU with the system CAN bus, if that matters.
Thank you.
-Mark