Part Number: AM2634
Hello,
I try to integrate the mcal driver. When I execute the CanApp driver I cannot see any messages on the bus. I just disabled the loopback test and let run the code. On the Port cfg file there are 47 ports configurated but there is no can related pins; also, the standby pin for receiver is not configurated.
Do you have the same issue?
Do I have to care another issue? I just want to run the CanApp code.
Thanks